Start Freq
Sets the frequency at the left side of the graticule. While adjusting Start Freq, Stop Freq is held constant, which means that both Center Frequency and Span will change.
Start Freq also sets the frequency entry mode to Start or Stop. In Start or Stop mode, the start frequency and stop frequency values are displayed below the graticule, and the default active function in the Frequency menu is Start Freq.
Remote Command |
[:SENSe]:FREQuency:STARt <freq> [:SENSe]:FREQuency:STARt? |
||||||||||||
Example |
:FREQ:STAR 200 MHz :FREQ:STAR? |
||||||||||||
Notes |
Max value depends on Hardware Options |
||||||||||||
Dependencies |
By direct entry:
If you try to do any of the above, Stop Freq changes to maintain a minimum of 10 Hz for the difference between Start Freq and Stop Freq With the knob or step keys:
Start Freq can be limited by Span limits, if Stop Freq is below its preset value If the electronic/soft attenuator is enabled, any attempt to set Start Freq such that Stop Freq would be >3.6 GHz fails, and results in an advisory message. If the equivalent SCPI command is sent, this same message is generated as part of a “-221, Settings conflict” warning If Source Mode is set to Tracking, and the Max or Min Start Freq is therefore limited by the limits of the source, a warning message is generated, “Data out of range; clipped to source max/min” if these limits are exceeded. Note that for an external source, these limits can be affected by the settings of Source Numerator, Source Denominator, and Power Sweep |
||||||||||||
Couplings |
The four parameters Center Frequency, Start Freq, Stop Freq and Span are interdependent, as changing one necessarily affects one or more of the others. The couplings between Center Frequency and Span are detailed under the control descriptions for those controls. These couplings also affect Start Freq and Stop Freq |
||||||||||||
Preset |
Start Freq does not preset. On Mode Preset, Span & Center Frequency preset, and Start Freq is derived. On Meas Preset, only Span presets, but Center Frequency does not, so Start Freq will vary depending on Center Frequency When Mode Preset is performed while in External Mixing, the Start frequency of the current Mode is set to the nominal Min Freq of the lowest harmonic range in the Harmonic Table for the current mixer setup Note that, if the current measurement has a limited Span available to it, and cannot achieve the Span shown in the table (Span = Stop Freq – Start Freq), the instrument uses the maximum Span the measurement allows, and sets Center Frequency to the midpoint of the Start Freq and Stop Freq values in the Harmonic Table. Thus, in this case, Start Freq presets to a frequency below the preset Center Frequency by ½ of the maximum Span When Restore Input/Output Defaults is performed, the mixer presets to the 11970A, whose Start frequency is 26.5 GHz Therefore, after Restore Input/Output Defaults, if you switch to External Mixing and do Mode Preset while in Spectrum Analyzer Mode, the resulting Start Freq is 26.5 GHz |
||||||||||||
State Saved |
Saved in instrument state |
||||||||||||
Min |
-80 MHz, unless Source Mode is set to Tracking, in which case it is limited by the minimum frequency of the Source
If the knob or step keys are being used, depends on the value of the other three interdependent parameters While in External Mixing, the minimum Start Freq you can set is determined by the external mixing parameters. It will be close to the minimum LO frequency (3.8 GHz if undoubled, 8.6 GHz if doubled) times the harmonic number, for the lowest harmonic range in the Harmonic Table for the current mixer setup. It can be queried with :FREQ:STARt? MIN |
||||||||||||
Max |
Depends on the instrument maximum frequency – 10 Hz. Note that, if Source Mode is set to Tracking, the effective instrument maximum frequency may be limited by the source maximum frequency If the knob or step keys are being used, it depends on the value of the other three interdependent parameters While in External Mixing, the maximum Start Freq you can set is determined by the external mixing parameters. It will be close to the maximum LO frequency (7 GHz if undoubled, 14 GHz if doubled) times the harmonic number, for the highest harmonic range in the Harmonic Table for the current mixer setup. It can be queried with :FREQ:STARt? MAX |
||||||||||||
Annotation |
Start <value> appears in the lower left corner of the display. This replaces Center <value> |
||||||||||||
Status Bits/OPC dependencies |
Non-overlapped |